Custom Analytics Solutions
WAGO Analytics

When it comes to optimizing a system, the challenges lie in improving and quantifying knowledge of the process and incorporating the results back into the process. WAGO Analytics supports you from data acquisition to analysis and creates intuitive visualizations of dependencies in the systems. The interrelationships it uncovers can be incorporated into the processes, allowing you to exploit potential for optimization.

In joint projects, WAGO works closely with customers to develop tailored solutions for the profitable data use within the specific application.

The Benefits for You:

  • Identification of optimization potential
  • Improved quality level
  • A tailored analytics solution
  • Greater efficiency and lower costs
  • Improved process stability

Six Steps from Data Acquisition
to Profitable Use

MM-32100 _Iso_Grafik_Analytics_Process_6_Steps_B_2000x1125.jpg

WAGO Helps You Use
Your Data Profitably

We help you get the tailored analytics solution you need.

1. Gathering Raw Data from Various Data Sources

In the first step, the relevant data sources are identified together with the relevant domain expert. The various interfaces are read out independently of the respective protocol. Values are accessed from the controller directly, and additional sensors are installed if necessary. The analytics solution is integrated into the existing control system, so the automation engineering responsible for the system is consulted on the data acquisition setup.

2. Processing the Data

In the second step, the data is time-synchronized. The relevant information is extracted and decoded in a uniform format. Irrelevant data is filtered out and removed. In addition, relevant metrics are calculated on an ongoing basis. This step is particularly important, because a clean database is the basis for the success of an analytics project.

3. Continuous Data Acquisition

In the following third step, an custom data logger is put into operation. The data is stored and used for in-depth analysis. A variety of useful data is generated through continuous data acquisition. This can be implemented in the form of test plans, together with the domain expert. Depending on the use case, it may also be sufficient to run the data recording over a longer period of time.

MM-4961_Analytics_Demonstrator_Screenshot_1_2000x1125.jpg

4. Explorative Data Analysis and Selection of the Right Representation

The fourth step involves exploratory data analysis and selection of the right representations. In offline analyses, dependencies and relationships are extracted, interpreted and visualized. Rare events are revealed. The close cooperation between the data scientist and the domain expert achieves the first successful identification of potential for optimization. Complex algorithms are often unnecessary. However, the exploratory data analysis also involves evaluating algorithms from machine learning and AI for different use cases in offline analyses. If the desired use case cannot be represented with the data from the existing database, either new sensors are installed, or the test plans are adapted.

MM-4961_Analytics_Demonstrator_Screenshot_2_2000x1125.jpg

5. Integration into the Operating Process

In the fifth step, the analyses and visualizations that have been optimized for the system are integrated into the operating process. Once again, the automation engineer is consulted about the integration into the control system.

6: Leveraging Correlations and Optimization Potential

In the sixth step, the customer exploits the interrelationships and potential for optimization, benefiting from the advantages of a tailored analytics solution. If necessary, the analytics solution can be expanded in a further iteration for the next use case.

MM-4961_Analytics_Demonstrator_Screenshot_3_2000x1125.jpg

Integrated Analytics for Industry

from Data Acquisition to Data Analysis

FAQ – Analytics

General Questions

How Can WAGO Analytics Benefit My Business?

Can an Analytics Solution Be Integrated into an Existing System?

How Much Data/How Many Data Records Do I Need When Starting an Analytics Project?

Do I Need a Cloud Service?

How Do I Monitor My Analytics Application during Operation?

What Methods Does WAGO Analytics Use?

How Do I Choose a Pilot Project?