Customer application
More Light, Lower Costs

When voestalpine, an Austrian technology and capital goods corporation, updated the lighting system at a central warehouse in Linz, Austria, the firm seamlessly switched to DALI-capable LED lights combined with proven WAGO Lighting Management. It was a great success: Based on the cost savings and the positive feedback from the workforce, they are already considering additional applications for WAGO’s solution.

Illumination is Often a Great Challenge

The illumination of warehouses and production facilities often entails a great challenge for manufacturers: The costs should be low, yet the lighting quality needs to be high in order to create optimal light conditions for the employees. If the economic aspects of lighting are prioritized, then energy efficient illumination must be considered in combination with an intelligent lighting management system.

The Austrian technology and capital goods company voestalpine has also been working on this topic for several years. The lighting control in the production facilities and warehouses has until recently been handled by using complex programs that were created for each building by external automation specialists and were linked to the specific demands for that site. The problem: The use of different programming languages that cannot communicate with each other has resulted in a situation in which centralized networking and control of the lighting systems are impossible. In addition, each new change in parameters requires knowledge of the programming language used. As the corresponding expertise is not always available to the necessary degree, the company depends on external service providers for more complex adjustments to the lighting technology.

building_referenz_voestalpine_gebaeude_nacht_2_2000x1500.jpg

The automated lighting control in the production halls and warehouses of the technology and capital goods company voestalpine is handled by WAGO Lighting Management.

Selecting a Pre-Programmed Web Solution

In the past year, the company went a step further and turned to a pre-programmed Web solution for their lights: WAGO Lighting Management. In the course of replacing the lighting in a central warehouse for steel rolls – each weighing several tons – the company chose to use automated lighting control in combination with the LED technology. Since then, the building in Linz, with an area of 5,400 m², has been illuminated by around 60 DALI-capable LED lighting units controlled by WAGO Lighting Management.

The challenges in this lighting management system are relatively straightforward in this initial project: It requires common, constant light control of all LED DALI lights with the aid of a brightness sensor in order to guarantee constant light levels at minimal energy consumption for all work shifts. The artificial light should automatically adapt to the natural light to optimally illuminate the building during every working hour, day or night. In addition, the individual operating modes, like “off,” “manual” and “automatic,” can be selected using a key-operated switch.

  • Automated lighting control in combination with LED technology
  • 60 DALI-capable LED lighting units controlled by the WAGO Lighting Management
  • Constant light regulation of all LED DALI lighting units with the aid of a brightness sensor
  • Constant illuminance with minimal energy consumption
  • The hall is optimally illuminated at all times, day or night, during the work week

Start Up before Lunch

All elements associated with the lighting management were defined prior to start up. The individual DALI lights and the DALI light sensors were read into the system using the implemented scanning and addressing functions. The conventional digital inputs for the key-operated switch were automatically recognized, as they were part of the internal bus system. In the next step, the virtual rooms stored in the software were named according to their respective building components. All previously defined elements, like key-operated switches, electronic DALI ballasts and DALI sensors, were allocated to the virtual rooms and assigned to the “constant lighting regulation” function. Subsequently, a variety of parameters were defined, for example, monitoring parameters, and adjusted to the specific application. All commissioning, including the function test, was carried out in a single morning.

building_referenz_voestalpine_lagerhalle_1_2000x1500.jpg

Simple Maintenance, Easier Parameter Setting

“After only a few months, it was clear that adapting the electric light to the daylight and using LED lights significant reduced the energy costs – even though the warehouse lighting level was actually increased,” reports Michael Haudum, who managed the project for voestalpine. In addition, maintenance on the new system is much easier. Haudum adds: “We can now change parameter settings in-house at any time without any additional programming effort or recourse to outside companies.” The WAGO Lighting Management system enables the voestalpine maintenance department to monitor all parameters using a modern, standardized Web visualization, and to adjust them at any time as needed. New parameters can be set quickly and easily with the click of a mouse – even during operation. The graphical user interface can be accessed by any standard browser in the internal voestalpine network. The system is based on the popular web language HTML5, so local software installation on a PC is unnecessary.

“Based on the successful implementation in our warehouse, we are planning to introduce the WAGO solution in other areas in the future,” says Haudum. This shows the high level of flexibility that can be achieved using WAGO Lighting Management. From a small facility with only one virtual room, up to multiple networked distributors with 160 virtual rooms, including links to the building technology, everything can be centrally controlled and automated according to custom specifications. Haudum is also considering expanding the application with new control functions in some places – for example, colored lighting control for control stations. “Basically, we see the simple, centralized controller, the standardized Web interface and the energy cost savings as the essential advantages of the WAGO Lighting Management,” says Haudum.

WAGO Lighting Management – the Benefits for You:

  • Easy usage and document creation

  • Innovative operating concept using standard Web browser

  • Well-organized input screen

Text: Martin Morpurgo and Michael Gerner | WAGO
Photo: Voestalpine

WAGO at Work

More Building Technology Applications

As a partner and innovation leader, WAGO implements many interesting projects. Learn more about our creative and efficient building technology solutions.

New Lighting Standard Reduces Energy Consumption

BMW has been able to cut energy costs in their production halls by about 30 %. The solution, based on WAGO components, is now a company-wide standard.

building_referenz_produktionshalle_bmw_2000x1500.jpg

Innovative Lighting in the Office

Philips, a technology company, has created a showpiece for innovative lighting and building management using flexROOM® from WAGO.

building_referenz_philips_arbeitswelten_3_2000x1500.jpg

Recommended Reading

More Building Technology Applications

Whether you are planning lighting installations and automation in your office building, retrofitting a heating, ventilation and air-conditioning system or involved with room automation, WAGO helps you meet your requirements in buildings.

Intelligent Room Automation and Installation for Greater Efficiency

The planning, implementation and operation of a building must demonstrate both maximum efficiency and a high degree of adaptability.

building_raum_innen_grossraumbuero_leer_1_Fotolia_74441791_X_2000x1500.jpg

Certified Buildings

Sustainable construction pays off. Several certificates provide planning support – one of which accounts for the potential energy savings of building automation.

building_raum_gebaeude_fassade_himmel_blau_istock_000048706942_2000x1500.jpg

This May Also Interest You

WAGO in Other Industries

Lighting Technology

From connection technology for LED modules and drivers, to lighting connection and lighting management, WAGO has the experience and solutions to help you implement lighting efficiently and effectively.

wago_brancheneinstiege_lighting_wglow_2000x1500.jpg

Power Engineering

The energy sector is facing great challenges in every area. Intelligent networking and innovative solutions from WAGO help meet these challenges.

Energy_FINAL_V6_2000x1500.jpg