[ { "uid": "link_contact", "linkName": "Contact", "url": "/mx-en/contact", "target": "_self", "classAttributes": "phone" } ] [{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]

Topics
Cybersecurity on Ships

With increased digitization and networking aboard ships, the risk for data abuse and cybercrime also increases. Anyone considering the possibilities of Maritime 4.0 must also consider the increased requirements for cybersecurity – and more importantly, find suitable solutions for implementing it.

A ship's various intelligent subsystems ensure problem-free operation: from tank and ballast water management through drive control up to alarm and monitoring systems. They all function using industrial automation technology.

Cybersecurity on Ships – This Is How WAGO Helps:

  • As networking in the marine sector increases, so does the exchange of sensitive data.
  • Electronics such as navigation, tracking and collision warning systems require off-ship connections, thus creating a potential target for cybercriminality. With “IT Security by Design,” a layer-based security architecture is integrated into the controllers from the start.
  • WAGO establishes such VPN tunnels using OpenVPN or IPsec directly from the WAGO PFC200 Controller, for example.

Data Security in Focus

At many points, advantages result from networking these subsystems – for example, when ship operations can run with greater resource or energy efficiency. The exchange of sensitive data also increases everywhere systems are networked. And yet this is not enough. In comparison to applications on land, ships have additional electronics like navigation, tracking and collision warning systems. They serve the safety of the ship; however, they also represent an additional threat, primarily because they not only increase the level of onboard networking, but also establish external connections. Internet-based network technologies or mobile services are seeing greater use for these connections. And these communication paths provide access points for manipulation – particularly at the points between the ship and land.

Functional Safety at Risk?

Access to or the reading of sensitive data is a comparatively less important problem when compared with the effects caused by hackers introducing malware into the control systems of ships or drilling rigs, altering coordinates, or accessing a vessel’s security-relevant subsystems. These acts don’t just endanger cybersecurity, they also impede functional safety, and ultimately the crew’s safety. This is precisely why recommendations regarding cybersecurity have increased along with the level of digitization and networking. The American Bureau of Shipping, the Baltic and International Maritime Council, Lloyd’s Register Group, the UK Chamber of Shipping, and the European Union Agency for Network and Information Society have all published guidelines regarding cybersecurity aboard ships. In general, they define processes, model approaches or technical measures for implementing cybersecurity; for the most part, these align with the guidelines for automation technology.

marine_grafik_maritim-4.0_cyber-security_2000x1125.jpg

The reasons for remote access vary greatly between shipping companies and OEMs.

“IT by Design” Instead of “Defense in Depth”

There also seems to be agreement that additional communication relations are generated by Industry 4.0 or Maritime 4.0, providing an increasing potential for cyberattacks. What is more important is that isolation concepts are reaching their limits. This is because of the opportunities provided by networking, which both increases the frequency of outside access and allows much deeper penetration into the ship's automation systems than before. There is a completely transparent reason for this: by using remote solutions, shipping companies obtain the possibility for remote diagnosis of their ships, which allows them to optimize their fleets and remarket the recorded data. In addition, they can reduce labor costs if fewer personnel or a less qualified crew is used that can receive support from engineers on land for repairs.

Why Permit External Access?

And finally, better networking of shipping companies and harbor unions improves the logistics at the docks and reduces fuel consumption for the ships. Simply preventing external access cannot be a solution for fixing security on ships. Defense in depth, however, which has previously been considered as state of the art, will soon become insufficient – even if it starts with access limitations, network segmentations and monitoring systems on the various levels of ship automation.
Security concepts are increasingly required that always function, regardless of the time or remote access point. The new demand is for “IT Security by Design,” that is, functions of cybersecurity that are integrated from the start into the configuration of a layer-based security architecture in the controllers.

marine_grafik_maritim-4.0_cyber-security_2_2000x1125.jpg

Typical systems on ships that use big data and have undergone increasing levels of networking.

From the PLC to the Cloud – Securing the Path that Data Takes

Such technical possibilities already exist and are capable of closing gaps in security. For example, a reliable means of communication is the establishment of a virtual private network (VPN), based on OpenVPN and using SSL/TLS connections (Secure Sockets Layer, Transport Layer Security). These connections enable the transmission of encrypted data, even over wireless communication systems. WAGO establishes such VPN tunnels using OpenVPN or IPsec directly from the WAGO PFC200 Controller. The WAGO controller additionally records all relevant measurement and control data, encrypts it directly in the controller using SSL encryption and transmits the data as VPN. This means that no additional VPN tunnels have to be established by modems or routers, and, what may be more decisive, the line between the controller and modem is then directly encrypted as well.

Text: Norman Südekum, Eva Bannholzer | WAGO

Photo: WAGO

WAGO at Work

Additional Topics from the Maritime 4.0 Area

How does shipping profit from digitization and which challenges must be faced? Discover additional exciting topics from the Maritime 4.0 area.

Interview

Remote Access on the High Seas

What would happen if there were a chance to deeply access the engine room level – even from afar? Andrea Grün, from DNV GL, provides answers.

marine_fernzugriff_gruen_2000x1500.jpg
Marine and Offshore

Big Data for Big Ships

What concrete opportunities, risks and challenges does Maritime 4.0 offer? WAGO has answers and solutions.

marine_dickschiff_maritim-4-0_big-data_1_2000x1500.jpg
Your contact person at WAGO

Headquarter Mexico

Vertrieb_kontaktmodul_kundenservice_vertrieb_mann_gettyimages_482100240_400x346

Additional service offerings:

Recommended Reading

More Marine Applications

Whether Maritime 4.0, propulsion control or tank ballast and cargo management – WAGO offers solutions for every maritime challenge.

Propulsion Control

Ready for Whatever Comes Next

Intelligent automation solutions also belong to future marine applications. Stay on the safe side with WAGO’s solutions.

marine_motorboot_segelyacht_gettyimages-556376575_2000x1500.jpg
Tank Ballast and Cargo

Perfectly in Balance

Maintaining stability in rough seas is vital for freighters. Reliable tank ballast systems are key to this – with solutions from WAGO.

marine_containerschiffe_oben_1_2000x1500.jpg
Deck Handling and Cranes

Safe Around the Clock

Maintenance-free and safe solutions to keep tugboats and cranes ready for action at any time. WAGO’s solutions prove their strength under the most demanding conditions.

marine_schlepper_seil_2000x1500.jpg
Alarm and Monitoring

Reliable Signal Processing

Collect, condition and visualize data and, when necessary issue alarms: WAGO-equipped alarm and monitoring systems get the job done.

marine_steuerraum_1_gettyimages-169263598_2000x1500.jpg

This May Also Interest You

WAGO in Other Industries

WAGO’s automation and electrical interconnection technologies are not only represented in the marine and offshore sectors. Learn what solutions WAGO offers in other industries.

Process Engineering

Always Innovative

Whether energy management or explosion protection, from Process 4.0 to cybersecurity, WAGO continuously develops solutions for users and planners.

brancheneinstiege_prozess_2000x1500.jpg
Building Technology

Make Plans Today for Tomorrow

Whether lighting and room management or solutions for heating, ventilation or air conditioning, WAGO is an innovative partner with the right products to save you time, costs and energy.

brancheneinstieg_gebaeudetechnik_2000x1500.jpg