Topics
Extremely Reliable Even Under Extreme Conditions

Whether encased in ice, surrounded by desert or on the high seas, components at pumping stations for oil and gas production must endure the harshest conditions for decades at a time. The WAGO-I/O-SYSTEM 750 XTR has been specially designed for these environments.

WAGO's controllers are used, not only in many aspects of industrial automation and processing technology, but also in pumping stations of diverse types. Pumps are used, for example, to lower ground water levels at mining and construction sites, and also form part of the supply infrastructures in all industrial manufacturing and process engineering. Another important and highly complex application appears in oil and gas production around the world, from Alaska and Russia to Brazil. In addition to processing all relevant parameters, like pressure, temperature and throughput, WAGO automation can take over the control of the pumping station itself, and also offers the option of connection to the control level.

Your Benefits at a Glance:

Unlimited automation in extreme environments:

  • The WAGO-I/O-SYSTEM 750 XTR simplifies maintenance
  • Reduces space requirements, as well as energy and maintenance costs
  • Increases system availability and return on investment
  • Enhances productivity

Products

The 750 XTR Controller

Extremely temperature-resistant, immune to interference, as well as unfazed by vibrations and impulse voltages: WAGO's 750 XTR Controller is the robust solution for small control tasks.

s_0750_XTR_Knoten_016_2000x1125px.jpg

Between Productivity and Environmental Protection

The components that are installed in pumping stations to extract liquid and gaseous raw materials have to withstand a wide variety of environmental conditions and must also satisfy the highest levels of legal requirements of different countries. In addition to strict regulations and controls by state institutions, the oil companies also have also incorporated strict guidelines for the selection, use and operation of components and assemblies into their specifications. These requirements concern not only system availability and productivity, but also environmental and resource protections.

Extreme Conditions in Oil and Gas Production

Oil and gas production is a fraught topic, not only in politics, but also technologically. The production plants must be erected in direct proximity to the oil and gas reservoirs. These locations are often remote from civilization and are rarely inhabited, as most are subject to extremely harsh weather conditions. In those places where humans cannot or will not live, sensitive electronic components, like controllers, isolation amplifiers and I/O modules, must endure extreme weather events, because high system availability is the be-all and end-all in the multi-billion dollar oil and gas industry. This applies even during the design of pumping stations, because making the correct decisions for the highest level of productivity and long-term use of components is a necessity when systems are expected to function effectively for at least ten to 30 years under harsh conditions. For vendors, this means extraordinary requirements that must be observed during the development and production of components.

Salt Water Accelerates Wear

Installations on the high seas like drilling rigs are exposed to extreme weather conditions. While the temperature may see only moderate fluctuations in the range from +5°C to +30°C, the salt air adheres to and clogs components. Rust and other corrosion damage follows shortly thereafter. External corrosion caused by saltwater can only be counteracted by high-quality components made from stainless steel. So-called interior corrosion is far more problematic and also more difficult to manage, because hydrogen sulfide, which occurs naturally during oil production, also attacks stainless steel. As long as the materials remain in motion, this rarely arises. The media mixture of gas, oil, water and sand is critical when pumps are not operating and the mixture stands in the lines for any length of time. Therefore, electrical components in offshore applications are installed in specialized control cabinets to protect them from external influences as far as possible. In addition, the installation spaces are ideally equipped with air treatment systems to remove the salt from the air and maintain the temperature at constant levels. These solutions significantly increase component lifecycles.

The Challenges of Heat and Cold

In desert regions, electronics are exposed to large temperature fluctuations: At some locations in the Sahara, or the Rub-al-Khali desert on the Arabian peninsula, days can see temperatures higher than +60°C, while the nights are still relatively cold. Temperature differences of 40°C within 12 hours are not rare. External control cabinets can heat up to far more than 60°C. In addition, there is a risk that dust and sand can clog the control cabinet filters.

Of all extreme conditions, cold is the easiest to manage. The greatest risk there is that condensation will form on the PCBs, due to the temperature fluctuations, and destroy them. In addition, electronic components can be damaged when exposed to below-zero temperatures for long periods. These problems can be countered relatively easily by installing heating systems, which then ensure constant temperatures in the control cabinet room.

The WAGO-I/O-SYSTEM 750 XTR Can Meet Any Challenge

In addition to the stresses that nature places on electronic components in pumping stations, there are ever more legal requirements prescribing certification according to specific standards. These vary by country. Likewise, the environment surrounding the installation, for example, on oil tankers and drilling rigs, or in classic oil derricks, can contribute to the demands on control systems. Vibrations, temperature fluctuations and many other factors all have to be considered.

The WAGO-I/O-SYSTEM 750 XTR was developed precisely for these extreme conditions, which prevail particularly in the process industry and marine applications. In addition to extreme temperature resistance, from −40°C to +70°C, the system is also resistant to vibrations caused by mechanical forces. It is designed for vibrations up to 5 g (50 m/s²), is shock resistant up to 25g (250 m/s²) and can be used at elevations up to 5,000 m. The enormous immunity to impulse voltages protects the I/O system's electronics against impulse voltages caused by switching actions and arcing of up to 1.0 kV (24 V modules) and 5.0 kV (230 V modules).

Impressive Across the Board

Due to numerous features and a robust construction, WAGO's 750 XTR prevails against mechanical and climatic forces, without additional protective measures. This reduces spatial requirements on the DIN-rail. The individual components have more than 16 channels on only 12 mm of installation space. Energy and maintenance costs are reduced, and productivity is simultaneously increased. The controllers can be programmed in the familiar CoDeSys environment per IEC 61131-3. The WAGO-I/O-SYSTEM 750 XTR thus facilitates optimal system availability under harsh conditions for many years, in addition to a maximum return on investment.

Text: Julia Grobe | WAGO

Photo: iSTOCK.com, WAGO

This May Also Interest You

More from the Process Engineering Area

Whether modular process automation, explosion protection, cybersecurity or Process 4.0 – WAGO offers solutions for every challenge facing the industry.

Process 4.0

Intelligent Value Chains

Digitally transform and reshape processes: WAGO is your reliable partner for individual development and implementation.

process_prozessindustrie_virtuell-real-welt_istock_101279527_2000x1500.jpg
Modular Process Automation

DIMA Is the Future

Modular systems concepts are the solution to constantly shifting market demands. WAGO supports your development process.

process_modulare-prozessautomation_gettyimages-457978501_2000x1500.jpg

Recommended Reading

WAGO in Other Industries

WAGO’s automation and electrical interconnection technologies are also popular beyond process engineering. Learn what solutions WAGO offers in other industries.

Underway on the Ship of the Future

Modern propulsion technology, networking subsystems – automation and digitization are standard on ships.
MM-4796_Website_Marine_Update_New_Fotolia_93216555_2000x1125_stage.jpg

An Industry in Transition

Modern automation and digitization technologies give rise to communicative smart grids.
brancheneinstiege_energie_2000x1125.jpg