Customer application
DIMA Leads to Smart Production

With DIMA, WAGO has developed a new, manufacturer-independent solution for automating adaptable production facilities. The goal of the approach is to allow modification of production systems within a short time. Thus DIMA combines the advantages of the modularity of production facilities with Industry 4.0 approaches that are currently under discussion.

The Digitization of Production

No other Western country is as oriented towards industrial production as Germany. In 2011, to prepare itself for the seismic shifts that are underway and take an active role in determining the outcome, the German federal government proclaimed the fourth industrial revolution: Industry 4.0. The focus is on digitization of production. But why? Digitization allows information to be linked in a way that generates added value. This added value can consist in revealing interrelationships, optimizing control in production processes or simplifying systems engineering. And there is an explicit need to simplify and accelerate engineering: If manufacturing companies need to adapt their product features on short notice in order to react to market changes, this ultimately also means that they have to convert their production facilities in order to produce the new product – and they generally do not have much time to do so.

Why Industry 4.0?

  • Networked information gives rise to added value.

  • Production processes can be improved.

  • Plant engineering is simplified.

  • Saving Time and Money

Industry 4.0 in Real-World Production Systems

Looking closely at today’s production systems, we quickly discover that they are not designed for the requirements of rapid conversion, simply because properties such as mobility, scalability, universality, compatibility and especially modularity were not taken into account in the initial application planning. However, modularity is a core requirement for adaptable production systems. There is a good reason for this: “Carving up” today’s monolithic systems into modules opens up a wide range of options. It becomes possible to easily adapt the production volume, relocate individual modules, carry out testing and perform run-in and acceptance at the R&D site, so the system can then be sent to the actual production site – without the need for trained engineers available at the production site.

Automation of Modular Applications

Ideally, the virtual map (AAS) of the production system should always correspond to physical reality – even within the process control system. If a new module is added, it should possible to represent it in the process control system without additional programming effort and use it immediately – very much in the spirit of a “plug-and-produce” paradigm. It’s obvious that such a system architecture requires a new approach to automation of systems: decentralized processing intelligence. Together with the Dresden University of Technology and Helmut Schmidt University of Hamburg, WAGO dedicated itself to this approach and presented DIMA (Decentralized Intelligence for Modular Applications) in November 2014.

DIMA shifts large parts of the control intelligence to the modules. These provide their intended function as services that can be accessed by other communication elements via a standardized interface. A module is still operated via control screens. Furthermore, the control screens are also described in such a way that they can be generated automatically in any target systems.

digitalisierung_wandlungsfaehigkeit_dima_industrie-4-0_01_einheitliches_bedienen_2000x1500.jpg

“Plug-and-produce” technology is edging closer. With DIMA, switching out system modules in less than three minutes is possible.

MTP Approach of an Administration Shell

The process for announcing the services and control screens is not based on proprietary solutions, but rather on a new description method – the Module Type Package (MTP). This serves as a digital description of a system module and contains all the information required for integrating the module into the system and then operating it. Modeling this capability description is the core of DIMA. The process function of the module (for example, the reaction of a reactor module) is modeled in the form of a service, i.e. a closed function, which is only addressed via its standardized interface. Thus the process control level becomes the service user. The services of all modules connected to the backbone and announced by an MTP are orchestrated in the engineering tool of the process control level.

digitalisierung_wandlungsfaehigkeit_dima_industrie-4-0_mtp-grafik_1_2000x1500.jpg

The MTP (Module Type Package) is the digital description of the system module and represents it in the process control system. It contains all the information necessary to integrate the module into the system and operate it.

MTP – an Initial Real-World Module

As the digital calling card of a system module, the Module Type Package (MTP) provides an initial approach to implementing the virtual representative in the information network. It already represents the application module’s functions and manages them within the architecture of the overall system. Thus MTP is an initial real-world module to meet Industry 4.0 requirements. However, the program code necessary for this service is executed in the module.

About DIMA:

  • Combines the advantages of the modularity of production facilities with Industry 4.0 approaches that are currently under discussion

  • System automation via a decentralized processing intelligence
  • Shifts large parts of the control intelligence to the modules

DIMA – the Solution for Modular Automation

The basic idea of this modular system architecture: integrate properly equipped modules with integrated automation into the overall system with minimal effort. It offers an open system architecture and allows cost-effective engineering of the entire system. Read about how DIMA drives adaptable, smart production here.

digitalisierung_referenz_sps-2016_christian-sallach_ulrich-hempen_thomas-holm_sven-hohorst_2000x1500.jpg

Inspiration for You

Read More about the Industry of Tomorrow

Cybersecurity

As digitization progresses, production data requires greater protection. WAGO helps you secure valuable data with smart products and solutions.

digitalisierung_2000x2000_140522-IT-108.jpg

Cloud Connectivity

Cloud solutions are becoming more are more popular in industry. They link the real and digital worlds, allow efficient use of production-related data and simplify cross-site networking.

digitalisierung_cloud-connectivity_mann_tablet_anlage_sichtfenster_GettyImages-556419007_2000x1500.jpg

Smart Data

Data software tools and interfaces combined seamlessly: From planning to delivery of a switchgear unit, WAGO’s Smart Data offers digital support for your engineering process.

digitalisierung_smart-data_zwei_personen_rechner_fabrikanlage_arbeitssituation_GettyImages-482172147_2000x1500.jpg