[{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]

Perfectly Plugged Electrical Installations – with WINSTA®

The WINSTA® Pluggable Connection System is perfectly tailored to the strict requirements of building installation. It allows simple pluggable connections, making electrical installation fast, safe and error-free. This is also true for other domains, such as marine and railway systems, as well as industrial applications.

winsta-gesamt_2000x2000px.jpg
Your WAGO Contact

Additional service offerings:

Avoid Errors and Save Time

In 2015, the Swiss Post relocated its headquarters to Wankdorf City, a business park in Bern, Switzerland. The imposing facility is located across the tracks from the commuter train station in Wankdorf. Elektro Burkhalter AG, the company responsible for the electrical installations, relies on the WINSTA® Pluggable Connection System from WAGO – and with good reason.

building_referenz_pitthan-elektrotechnik_winsta_2000x1500.jpg

Flexible Automation Instead of Expensive Conversion

The new SkyPort office and administration building at Stuttgart International Airport showcases a sustainable office complex. A solution that spans different building systems provides highly flexible room automation in the airport authority’s new headquarters.

building_referenz_skyport_gebaeude_2000x1500.jpg

Fashion Forward with WINSTA®

Zinser, a fashion house in Tübingen with a rich history, is undergoing modernization and will soon be brilliantly illuminated by 7,500 LEDs. To install the lights in the shortest possible time – and during ongoing sales operations, no less – Elektro Kürner GmbH relies on the WINSTA® Pluggable Connection System from WAGO.

building_referenz_modehaus-zinser_2000x1500.jpg

Pluggable Connection System in the Herford Hospital

Herford Hospital is being completely renovated, expanded and modernized. The hospital selected WAGO’s pluggable cable assemblies for the electrical wiring of the new, spacious one- and two-bed patient rooms. The factors tipping the scales toward WINSTA® included 70% less time and 30% lower costs.

building_referenz_klinikum-herford_gebaeude_2000x1500.jpg