Playing It Safe with the Power Supply
Protection with Fieldbus Couplers from WAGO
- Power Supply for Machines
- Remote Monitoring of the Circuit Breakers
- Alerts – Detailed and around the Clock
- Easy Retrofitting and Potential Expansion
There are multiple supply lines from the medium-voltage network on the Schweinfurt facility grounds. They supply the transformer substation, which has just under 100 transformers, and these in turn supply around 30 low-voltage main distribution boards, which provide the power to the facility’s manufacturing machines. “Power supply safety and reliability is particularly important to us,” explains Julian Kübler, who is responsible for monitoring the medium- and low-voltage transformers at the Schaeffler factory in Schweinfurt. Circuit breakers separately isolate the outputs for the electrical loads in the systems. Each circuit breaker is accommodated in a control cabinet in its own array. For loads with lower power, several small circuit breakers are sometimes mounted in an array. A typical system consists of two to three regions with 15–20 arrays with a total output of up to 2,000 kVA.
The employees can monitor the status of all circuit breakers at all times from the control center, which is installed in the maintenance workshop. The status of the entire power supply is transparently visualized here. The new fault message system, which has been installed in three of the low-voltage systems so far, provides significantly more functions than the previous solution. In case of a fault, the maintenance employees know which circuit breaker has been triggered and which malfunction is located where. The security center likewise receives more detailed error messages and can thus provide the on-call service workers with important information before they arrive at the facility. “In this way, we can increase the safety of our low-voltage power supply, and thus the uptime of our production systems,” says Kübler happily.
by Frank Sünkel | 2016-10-12
Photos: Anand Anders/vor-ort-foto.de
WAGO at Work
Customer Applications from the Area of Production Technology
As a partner and innovation leader, WAGO implements many interesting projects. Learn more about our creative and efficient production technology solutions.
Recommended Reading
More Solutions
WAGO’s automation and electrical interconnection technologies are not only represented in production technology. Learn what solutions WAGO offers in other industries.