These are good reasons for ESFORIN to rely on WAGO products for their projects. WAGO Cloud functions as a platform to output the algorithm commands to customers’ control systems; the WAGO PFC100 and PFC200 Controllers work to quickly and securely deliver the request signals to the customer systems. In addition, they back up data from the signals into the cloud. “In light of our responsibility for securing the electrical supply, there is no doubt that we use industrial-grade components, which have been tested over the long term and function reliably,” says Gardlo. Geyer confirms this fact, “After a year’s experience with the system, we can truly say that it works.”
For ESFORIN, a central benefit of using WAGO Controllers lies in their wide variability. “While these products are standardized hardware, they are, due to an extensive range of interfaces, sufficiently flexible to easily handle the heterogeneity encompassed by our customers’ process control technology,” explains Gardlo. WAGO’s Cloud Connectivity Protocol guarantees seamless connection to the cloud. After consulting with system operators about the data points to be transferred in both directions, ESFORIN runs proprietary software on the controllers to ensure communication. The customers then install the controllers in their control centers. “WAGO's controllers can be implemented as plug-and-play components. This corresponds to our approach of burdening our customers with the least amount of effort,” states the ESFORIN CEO.
WAGO Cloud, operated using Microsoft Azure, also ensures that the tens of thousands of commands, output daily by the ESFORIN algorithm, are correctly delivered to the customer systems in the available time intervals – thus virtually in real-time. This is one of the more unusual applications of WAGO Cloud because many use it as a data hub. ESFORIN’s applications demonstrate, however, that it also reliably satisfies these demands.