Hand in Hand for Ex Protection

Ex protection is definitely a topic most system manufacturers and operators do not enjoy discussing in detail, due to its extreme complexity. But not Quintex! Ex protection is their “daily bread.” This highly specialized company provides installation-ready junction boxes for ex zones, which solve this vexing problem for system manufacturers and operators. Quintex housings always include WAGO rail-mount terminal blocks and the WAGO I/O SYSTEM 750.
Explosion protection originated in mining. This was a dangerous profession up until the second half of the nineteenth century. In the meantime, explosion protection has also spread to other industries. Examples include the chemical industry, the production of crude oil and natural gas, the food industry and biogas systems – anywhere that gases and dusts are generated that create a “dangerous explosive atmosphere” when combined with oxygen. If ignition, caused by a hot surface or an electrical spark, is applied to these mixtures, then a situation could quickly arise that absolutely must be prevented: an explosion, which may potentially injure many people.
The WAGO I/O SYSTEM 750 XTR ‒ the Benefits for You:
Fieldbus-independent, flexible and robust
Carries all internationally relevant approvals
Compact design favors use in tight spaces