[ { "uid": "link_contact", "linkName": "Contact", "url": "/us/contact##wago-support-contact-anchor", "target": "_self", "classAttributes": "phone" } ]
[{"term":"Libraries_BA","id":0,"type":"QUICKLINKS"},{"term":"Instructions","id":1,"type":"QUICKLINKS"},{"term":"WAGO-I/O-PRO","id":2,"type":"QUICKLINKS"},{"term":"Building","id":3,"type":"QUICKLINKS"},{"term":"221","id":4,"type":"QUICKLINKS"}]

Topics
Intelligent, Efficient Plant Control

Both Ex and non-Ex areas can be found in wastewater plants. The WAGO-I/O-SYSTEM 750 allows efficient plant control for both areas.

Several specialized and general regulations complicate the construction and operation of a wastewater plant, making it anything but easy. Planners and operators can significantly lower their expenditures by selecting an intelligent control system that supports standard and special applications equally.

WAGO-I/O-SYSTEM 750 Advantages:

  • Ex and non-Ex area covered by one system
  • Intrinsically safe, fieldbus-independent, flexible and robust
  • Compact design encourages use in limited spaces

Chemical Reactions Possible at Any Time

One thing is for certain: It is almost impossible to predict the composition of the effluents arriving in wastewater plants. Contaminations, flammable compositions or chemical reactions can occur at any time due to accidents or unauthorized discharges. These may result in outgassing, which must be classified as a hazardous atmosphere. If highly flammable liquids, such as gasoline, get into the sewer system, they will float on the surface due to their lower density. As volatile materials, they evaporate quickly; depending on their concentration, they can create a harmful or even explosive mixture. Since the vapors that are generated are often heavier than air, they inevitably collect at the lowest point of the sewer network. Therefore, the sewer network and its structures, such as enclosed storage basins for wastewater, stowage canals, pumps or inverted siphon structures, are classified as Zone 1 or Zone 2 depending on their design.

Correctly Classify Zones

Whatever applies to the sewer network also applies to wastewater plant purification systems. These systems often consist of a wastewater pumping station and a discharge structure to help guide the effluents directly into the sewage treatment plant. If the structures are enclosed, then they must be classified as Zone 1. This requirement can also apply to open structures if they do not have any ventilation. Easily explosive mixtures can even be generated inside, for example, due to the completely normal outgassing of the effluents. This is because sludge gases are generated by fecal matter, which is a major part of the wastewater. However, sludge gases are only slightly lighter than air, and they do not collect in the upper areas of rooms or structures, but rather mix with the air. The exact composition of the air–gas mixture created in this manner cannot be determined – the continuous movement of the wastewater always generates new turbulence in the air. Thus, the gas concentration within the air–gas mixtures changes constantly.

process_grafik_Explosionsschutz_Abwasseranlagen_2_2000x1125.jpg

High Concentration of Sludge Gases

A very high concentration of sludge gases is actually related to the function of the rake structure, because coarse and fine materials, such as tree branches, textiles and hygienic items, are separated here. Accordingly, this area is classified in the hazard assessment as Zone 1 and adjacent areas as Zone 2. This classification also applies to sludge water reservoirs, such as shafts and structures, of the de-sludging step. The anaerobic bacterial processes, active during sludge decomposition in the wastewater, are used in the digester tower of the sewage treatment plant to extract sludge gases. These sludge gases will be converted into electricity and heat in a downstream block heat and power plant to positively impact the wastewater treatment plant’s energy balance. The process areas, from sludge thickening up to sludge decomposition, are also classified as Zone 1 and Zone 2 as part of the hazard assessment; The same applies to the outer areas of the sludge and gas container.

Build and Automate According to Standards

Based on these challenging everyday conditions, adhering to applicable standards and regulations including ATEX, IECEx and the industrial safety regulation (BetrSichV), is required. This is in addition to constructional elements for reducing the explosion hazard. Based on these standards, the operators of waste water plants are obligated to generate an explosion protection document for the hazardous areas of their plant. This document specifically defines the explosion hazards and specifies detailed protection concepts. Germany’s DWA bulletin 217 (DWA-M 217), titled “Explosion protection for technical waste water plants” (July 2014), provides useful information about the practical implementation of these requirements. These relevant standards and approvals must also be used for the design of the electrical equipment of a technical waste water plant; this also applies to the equipment of control cabinets.

process_grafik_Explosionsschutz_Abwasseranlagen_1_2000x1125.jpg

Two Zones – One System

Both the planner and operator are usually interested in minimizing the number of components and systems that must be used. For good reason: The complex requirements the waste water plant places on the control system impact the foreseeable expenditures for planners and operators, from initial engineering to eventual maintenance. Accordingly, they prefer products that can be used in both standard applications and hazardous applications, such as the highly aggressive or corrosive environments typically found in sewage treatment plants.

Trouble-Free Plant Expansion

WAGO has designed its 750 Series I/O System in such a way that the same platforms are used in the Ex and non-Ex areas. Clever details make the system extremely versatile without abandoning its overriding standard. Featuring 500 different modules, it offers the option of directly integrating different sensors in the field and transmitting very different forms of analog or digital signals bundled through TCP/IP to the control room. In addition, the WAGO-I/O-SYSTEM makes it possible to remotely record error messages or fill levels of rain overflow basins for controlling inflow into the wastewater treatment plant. In addition to fieldbus independence and standard availability of open interfaces for measurement technology, as well as the integration of entire system parts, WAGO also offers HART communication. Ultimately, this communication compatibility also makes future system expansions easy.

process_grafik_Explosionsschutz_Abwasseranlagen_3_2000x1125.jpg

Less Time and Effort for Planners and Operators

WAGO’s modular components enable planners to equip applications in the Ex and non-Ex areas economically and efficiently without extensive programming. Operators can also implement special solutions, such as partial energy measurement and storage of all process data, with the components of an automation system. This makes it possible to establish a targeted monitoring and management system that will display historic values. WAGO’s I/O system also provides function libraries for water and process systems free of charge, benefiting both the process engineer and programmer.

Author: Kay Miller

Your WAGO Contact

Technical Support-Automation

unternehmen_technischer_support_gettyimages-519425930_450x450

Learn more about WAGO within the industry here: