Customer application
New Brilliance for the Stadiums of Tomorrow

Following general renovations started in August 2020, the Helsinki Olympic Stadium now gleams with new light – literally. The SIRIUS® floodlight fixtures from SITECO, a lighting manufacturer, are responsible for this change. The company from Traunreut in Upper Bavaria, which is known for its tradition of quality, has set a new standard with these floodlights, now in use in stadiums around the world. SITECO integrates quality holistically. Because of this, the company relies on high-grade lighting connection technology from WAGO, which can be easily and intuitively operated due to the levers.
The SIRIUS® floodlight fixtures from SITECO will clearly spotlight future major events at the Helsinki Olympic Stadium – both for the 36,000 spectators in the stadium and the millions watching on their TVs. The especially precise lighting control is achieved through high-efficiency silver reflectors. Specialized Cut-Off variants trim superfluous light scatter and, at 96 points on the “Television Lighting Consistency Index” (TLCI), focus it precisely where it is needed – down into the arena, instead of up at the night sky.
WAGO PCB terminal blocks with levers provide:
Comfortable and secure connection in the field without tools – thanks to WAGO’s lever technology
High current carrying capacity in a compact construction, as well as flexible design-in potentials
Reliable, high-quality spring connection technology for numerous conductor cross sections – available worldwide