Connecting DALI Sensors
Space-Saving Connection in a DALI Line
Space-Saving Connection in a DALI Line
DALI sensors are primarily supplied via the two-wire DALI cable (DA+ and DA-). In some projects, “mixed” operation of DALI lights and sensors is not desired within a DALI line. In these instances, the space-saving two-pole MINI system is recommended for connecting DALI sensors. The two-pole DALI line is supplied by the DALI master via standard installation cable (1) from the subdistribution board. The two-pole WINSTA® Socket and Strain Relief Housing (2) are mounted on the standard supply cable. Two-pole T-distribution connectors (3) are used for integrating the DALI sensors (5) into the DALI line. Two-wire interconnection cables (6) to the through wiring and connecting cables (4) are used on the T-distribution connectors for connecting DALI sensors (5). The sensors (5) are connected with the free end of the connecting cable (4) at the jobsite.
WAGO at Work
Additional Instructions for the WINSTA® Pluggable Connection System