Intelligent local network stations (iLNS) can also play an important role in digitization of the network. Earlier transformers were passive elements that stepped down the electrical voltage from the medium-voltage network to the lower voltage used by the local supply network using a fixed ratio. An iLNS, in contrast, records various measurement kinds of data in the medium-voltage network and offers the option of reading these values out remotely. This allows the network operators to adjust the voltage levels at any time. For example, if, on a sunny day, a lot of solar power is supplied, which increases the voltage, an iLNS can quickly compensate for this. This increases the accommodation capacity of the network and prevents bottlenecks, which can ultimately put the brakes on the expansion of renewables. WAGO’s developments help promote the digitization of the energy supply. In order to convert conventional local network stations into intelligent ones, it is essential to synchronize the primary and secondary components in a reliable way that conforms to standards.
In conjunction with their project partners, WAGO has already created a corresponding system and completely equipped it with automation technology. The station uses a PFC200 XTR Controller for the medium voltage, a PFC200 Controller for low voltage, an e!DISPLAY panel for visualizing the measurement and control data directly at the LNS and completely automated connection technology. The WAGO Controllers, which are freely programmable via CODESYS, collect all data from the substation’s various systems via digital and analog signals (e.g., via Modbus RTU). These controllers then translate the data into supplier-required communication protocols (IEC 60870-5-101/-104 or IEC 61850) and transmit the data to the control center via data lines. In the opposite direction, the control center can access the substation’s systems, such as the medium-voltage control cabinet, protective devices or measurement systems from different manufacturers, using the WAGO Controllers.