OOO “SSTEnergomontazh” is part of the “SST - Special Systems and Technologies” corporate group, the market leader in the field of planning and installing cabled trace heating systems for both the private and the industrial sectors. The corporate group’s Russian plants is Europe’s largest producer of heating cables and technical equipment for temperature regulation. Since it was founded in 1991, the corporate group has installed more than 4,000 industrial trace heating systems in structures or on their roofs and more than 6,000 systems on pipelines and reservoirs. Trace heating systems from SST currently help ensure reliable operation of more than 20,000 kilometers of pipelines. The systems maintain a set temperature for products in pipelines and reservoirs.
To ensure that trace heating systems can continue to perform reliably at temperatures as low as −55 °C, several types of special heating cables are installed between the pipeline and its thermal insulation. Both heating cables designed for a constant temperature level and self-regulating cable systems are used. Self-regulating cable systems release their heat based on ambient environmental conditions. The advantages of these types of cables over cables with a constant level: Even objects with only a small area can also be heated, and with considerably greater energy efficiency.
Control cabinet for controlling industrial electrical trace heating systems.
Sensors and temperature regulators which monitor the temperature and control heating operation are also installed directly on the pipeline. One of OOO SSTEnergomontazh’s main goals is currently the use of automatic control and regulating systems for operating these systems. First of all, SST intends to develop this to fulfill customer-specific demands and offer tailor-made solutions. Secondly, the company is following the clear trend toward automation within the oil and gas industry: More automation for the product extraction and transportation – within both existing systems and new systems under construction. The goal is to provide every technical process – including heating – with options for self-diagnostics, output of relevant information to an HMI, signaling of messages in emergencies and status reports, as well as the acquisition and archiving of information required for proper operation. Control systems must be able to employ the latest communication protocols, transmit data to the process control system via digital interfaces, be used via the SCADA telecontrol protocol and offer control station and emergency-off functions. They must also be reliable and help enhance energy efficiency on the basis of optimized calculation algorithms and well-tuned system settings.
OOO SSTEnergomontazh chose to partner with WAGO in order to take a great step forward in automating electrical trace heating systems. SST uses several function modules from the modular WAGO-I/O-SYSTEM 750, including its explosion-proof modules. “There were very few companies that could offer comparable equipment at a comparable price,” says A. W. Mochow, head of the department for planning of electrical equipment at SSTEnergomontazh. “The product range for most manufacturers usually only covers components for use in industry.” However, in systems used for heating industrial facilities, the temperature must be monitored using sensors installed directly on the pipeline.
TEPLOMAG industrial electrical trace heating system during assembly.
This measurement point is located in hazardous areas of Hazard Category 2 and is also around one kilometer from the control cabinet, which is not located in a hazardous area. For this type of application, SST chose the 750-485 Function Module of the WAGO-I/O-SYSTEM, which connects to temperature sensors that are designed to use standardized current level signals. “This enabled us to retain fail-safe circuits without installing additional barriers,” explains Mochow. “We were also able to save up to 20 % of the space available in the control cabinets.” Another argument in favor of WAGO’s solution: Programming WAGO systems using CODESYS. Not only is this programing environment the most widely used and most universally applicable topology, but it “also offers a wide range of options for implementing algorithms tailored to the electrical trace heating field,” explains Mochow.
The head of SST’s engineering department has become a great fan of WAGO. He describes the company’s product support as top-notch and happily takes advantage of continuous updates to the range of products and the new program libraries made available to customers. “We constantly follow new developments at WAGO and have a close business relationship with their office in Moscow.” SST employees attend seminars and stay in touch with WAGO through regular meetings at international trade shows. And, in the end, Mochow feels that the success of this collaboration is what really counts. “Practical experience has proven that our expectations of WAGO have been completely met. Presently, we are operating numerous reliable systems throughout the corporate landscape of the Russian oil and gas industry.”
Extreme ambient temperatures
Immunity to electromagnetic interference and impulse voltages
Vibration and shock resistance
Explosion protection
Author: Benjamin Böhm | WAGO
WAGO at Work
Customer Applications: Explosion Protection
As a partner and innovation leader, WAGO implements many interesting projects. Learn about the creative, efficient solutions we make possible in the process engineering area.
Feige FILLING GmbH is a leading producer of filling machines for free-flowing products. It designs Ex solutions for ATEX category 1 with WAGO technology.
Contamination, vibrations, heat: As the controller for their mixed load system, Demostene + Partner AG chose a WAGO solution, which can handle anything.
In bituminous coal mining, only equipment with no danger of ignition is permitted. That’s why HAZEMAG & EPR relies on WAGO Controllers.
This May Also Interest You
More from the Process Engineering Area
Whether modular process automation, explosion protection, cybersecurity or Process 4.0 – WAGO offers solutions for every challenge facing the industry.
Adaptable production processes are the key to flexibility, efficiency and lot size 1. With WAGO, production modules can be combined in a customized and manufacturer-independent way.
Saving energy is good for the environment and for business. Performing the right analysis and taking the right steps can lead to sustainable profit. WAGO is your partner for effective energy management.
Digitization of ordering and production processes is a great opportunity for all companies. WAGO helps you take full advantage of this potential.
Recommended Reading
WAGO in Other Industries
WAGO’s automation and electrical interconnection technologies are also popular beyond process engineering. Learn what solutions WAGO offers in other industries.
Marine and Offshore
Modern propulsion technology, networking subsystems – automation and digitization are standard on ships.
Power Engineering
Modern automation and digitization technologies give rise to communicative smart grids.