Customer application
Safely Fill Explosive Substances in EX Areas

Filling above-level, sub-level or below bunghole – this is what you hear when experts talk about drum filling technology. Feige FILLING GmbH – headquartered in Bad Oldesloe, Germany – is an international leader of filling machines for liquid and pasty products. Since their filling machines mainly operate in hazardous areas, Feige FILLING, located in the Northern German state of Schleswig-Holstein, develops Ex-proof solutions for ATEX Category 1. To meet these requirements, the manufacturer relies on the universal WAGO 750 I/O System at the I/O level.

They may be green, gray, red, blue or black, but they always contain 200 liters. Internationally standardized steel drums are widely used to fill potentially hazardous liquids, such as oils and chemicals, into robust packaging. To fill these drums, Feige FILLING has developed a turnkey filling line that also includes both handling and material flow processes. “Our customers want to fill and ship their products. They do not want to worry about how the drums arrive under the fill valve or will later materialize on the shipping pallet,” says Marketing Manager Martina Thomsen. She adds that drums are just one of many packaging types that the Feige FILLING systems can accommodate. “The spectrum ranges from 1 m³ IBCs and drums to small containers, such as paint buckets from the hardware store.”

Safe Filling in Hazardous Areas

Given the variety of packaging, it is no surprise that the contents are also incredibly diverse, which is reflected in properties – high viscosity, foaming, combustible, or explosive – that can make the filling process extremely demanding. Therefore, Feige FILLING’s systems must meet particular requirements, including ATEX directive requirements that spell out the criteria for the construction and operation of machines and systems used in hazardous areas. About half the filling systems that leave the company are approved for Zone 1 hazardous areas, because explosion protection is part of Feige FILLING’s daily business. Fittingly, Feige FILLING considers this fact when configuring a system: “We place both inputs and outputs as close as possible to the process, where the signals are created and where they are transmitted,” explains Jörn Czysch, Automation Engineer at Feige FILLING. “Our goal is avoiding unnecessary wiring.”

Integrating the I/O Level Directly into the Process

When automating the filling process, Feige FILLING relies on WAGO’s intrinsically safe I/O modules from the WAGO 750 Remote I/O System. The modules can be installed close to the filling process for bundling sensors and light barriers on the input side, and solenoid and pneumatic valves on the output side. This allows Feige FILLING to save both installation space and time by bringing the control system close to the process. Compared to star topology wiring, the control cabinet’s position within a production line simply matters less. This reduces engineering costs while simplifying the design of modular systems. Another clear advantage of this proximity of control system to the process level is related to explosion protection, as the energy stored by systems providing intrinsically safe signals in hazardous areas must always be limited. For this purpose, distributed systems are much better because shorter cable runs simply store less energy. “Cables are potential energy storage units, which is why we always keep the length of cable runs in mind,” explains Czysch, an expert at Feige FILLING.

process_referenz_explosionsschutz_feige-filling_blaue-module_i-o-system-750_2000x1500.jpg

The blue WAGO 750 I/O System variants are designed for Ex applications. These are powered by a special supply module that also simultaneously serves as a separator for the non-hazardous level.

High Availability through Standardization

The advantage: From an engineering perspective, only one solution is used for system automation – regardless of whether the devices are connected in hazardous or non-hazardous areas. “It is extremely important that our system designs are very similar to each other,” says Axel Frank, Head of Automation Technology at Feige FILLING. “Maximizing the standardization in our system equipment ultimately helps us minimize the failure probability of individual components.” Because the WAGO 750 Remote I/O SYSTEM readily covers both hazardous and non-hazardous areas in one system, Feige FILLING can always equip the system automation with functional technology without leaving the stability of a standardized system.

Continuous Innovation Readiness

According to Czysch, there is one more advantage to working with WAGO, “We can rely on WAGO's willingness to innovate. WAGO kept advancing the 750 Series I/O System to provide us with new items and didn’t give up when additional requirements were needed.” To prove this point, the Feige FILLING expert referred to WAGO’s blue, intrinsically safe I/O modules for explosion protection and added, “They were not available when our partnership began.”

Text: Benjamin Böhm | WAGO

Photo: Thorsten Sienk

Product Overview

WAGO at Work

Customer Applications: Process Engineering

As a partner and innovation leader, WAGO implements many interesting projects. Learn about the creative, efficient solutions we make possible in the process engineering area.

Aircraft Fueling and Automation

Finally failsafe: Thanks to the switch to spring pressure connection technology from WAGO, the aircraft tankers at Brazil’s airports are safer than ever before.

process_referenz_rucker_flughafen_flugzeug_tankewagen_2000x1500.jpg

Automation for Pipelines

Trace heating prevents pipelines from freezing in Siberian temperatures. Explosion-protected components from WAGO play an important role.

process_landschaft_brunnen_schnee_2000x1500.jpg

Absolutely Reliable Quality

The requirements for the technical equipment aboard vessels are extraordinarily stringent. The WAGO I/O-System fulfills all of them.

marine_siem-pride_tatt_oktober_2000x1500.jpg

This May Also Interest You

More from the Process Engineering Area

Whether modular process automation, explosion protection, cybersecurity or Process 4.0 – WAGO offers solutions for every challenge facing the industry.

The Process Automation of the Future

Adaptable production processes are the key to flexibility, efficiency and lot size 1. With WAGO, production modules can be combined in a customized and manufacturer-independent way.

process_modulare-prozessautomation_gettyimages-457978501_2000x1500.jpg

Identify and Exploit Potential

Saving energy is good for the environment and for business. Performing the right analysis and taking the right steps can lead to sustainable profit. WAGO is your partner for effective energy management.

process_referenz_prozessindustrie-4-0_visualisierung_software_energiemanagement_tablet_produktion_halle_2000x1500.jpg

Smart Design for the Smart Factory

Digitization of ordering and production processes is a great opportunity for all companies. WAGO helps you take full advantage of this potential.

digitalisierung_smart-data_zwei_personen_rechner_fabrikanlage_arbeitssituation_GettyImages-482172147_2000x1500.jpg

Recommended Reading

WAGO in Other Industries

WAGO’s automation and electrical interconnection technologies are also popular beyond process engineering. Learn what solutions WAGO offers in other industries.

Marine and Offshore

Modern propulsion technology, networking subsystems – automation and digitization are standard on ships.

Marine_FINAL_V4_2000x1500.jpg

Power Engineering

Modern automation and digitization technologies give rise to communicative smart grids.

Energy_FINAL_V6_2000x1500.jpg