[{"term":"221","id":0,"type":"QUICKLINKS"},{"term":" Käyttöohjeet","id":1,"type":"QUICKLINKS"},{"term":" Kirjastot_Kiinteistöautomaatio","id":2,"type":"QUICKLINKS"},{"term":" Kiinteistöt","id":3,"type":"QUICKLINKS"}]
{ "@context": "https://schema.org", "@type": "BreadcrumbList", "itemListElement": [ { "@type": "ListItem", "position": 1, "name": "Kotisivu", "item": "https://www.wago.com/fi" }, { "@type": "ListItem", "position": 2, "name": "Ratkaisut", "item": "https://www.wago.com/fi/ratkaisut" }, { "@type": "ListItem", "position": 3, "name": "Sähkövoimatekniikka ", "item": "https://www.wago.com/fi/saehkoevoimatekniikka" }, { "@type": "ListItem", "position": 4, "name": "E-mobility", "item": "https://www.wago.com/fi/saehkoevoimatekniikka/e-mobility" } ] } [{"url":"/ratkaisut","name":"Ratkaisut","linkClass":null,"categoryCode":null},{"url":"/saehkoevoimatekniikka","name":"Sähkövoimatekniikka ","linkClass":null,"categoryCode":null},{"url":"/saehkoevoimatekniikka/e-mobility","name":"E-mobility","linkClass":"active","categoryCode":null}]
MM-438941_new-website-page_Application-Solutions_GettyImages-1390861566_2000x2000.jpg

E-Mobility Solutions

Electric vehicle (EV) charging is becoming important in the energy and mobility transition. Intelligent distribution of charging points and load management are central challenges to increasing e-mobility for network operators, facility managers and industrial companies.
Intelligent distribution of charging points and load management are central challenges in increasing e-mobility for network operators, facility managers, and industrial companies.

Load Management for Charging Infrastructure

Solution for Charging Point Management

Tailored but cost-effective – this is the core attribute of the WAGO Application Load Management software solution. It allows intelligent, sustainable EV charging with continuous power adjustment and utilization of all available capacity. It also boasts maximum scalability and compatibility with standard wallboxes and charging stations from many manufacturers.

One compelling feature is that a cloud connection, though possible, is not essential. Licensing is a one-time cost, and the application’s technical flexibility and technological interoperability support easy, cost-effective, sustainable integration into existing charging infrastructure. Thus WAGO Application Load Management allows renewable energy systems to incorporate additional loads and storage systems and use existing grid connections optimally.

Your Benefits:

  • Maximum compatibility and scalability 

  • Optional offline operation (if needed) 

  • Complete control over costs  

  • Prevent peak loads

Charging in Line with § 14a EnWG

Future-Proof Solution for Charging Parks: § 14a EnWG in Practice

Since the beginning of the year, § 14a of the Energy Industry Act (EnWG) has been in effect, providing grid operators with a tool to reduce output in case of network overload threats. While the supply of household electricity remains unaffected by this regulation, the use of energy-intensive systems such as heat pumps, energy storage units, air conditioning systems or wallboxes may temporarily be limited to 4.2 kW. This throttling has a direct impact on charging park management, requiring operators to implement necessary measures.

Power Reduction Through Throttled Charging

WAGO Application Load Management allows charging parks to be managed under the conditions set by § 14a EnWG. The system adapts to available power while maintaining remote control over charging systems. This makes WAGO Application Load Management an ideal solution for managing charging points when network power is reduced under § 14a EnWG. Charging capacities can be prioritized and allocated strategically, ensuring that critical charging needs are prioritized. Through Modbus, and in the future EEBus, it allows for precise power control between 0 and 100%, with eight configurable digital inputs.

Centralized management of all charging points: WAGO Application Load Management guarantees unified and efficient control, regardless of the charging infrastructure. This allows for smooth centralized control, even in mixed charging park environments. WAGO Application Load Management is compatible with and can be managed across various manufacturers.

Direct Connection to the Grid Operator

WAGO Application Load Management facilitates a direct connection to the grid operator using a comprehensive plug-and-play solution via a customer transfer station (KÜS). This standard setup enhances communication and data exchange between charging points and the grid operator, optimizing monitoring and control for operators.

For those aiming to be independent of § 14a EnWG, integrating PV and battery storage systems offers sustainable alternatives for future charging management.

Dynamic and Static Load Management

The focus is on compatibility and interoperability with standard wallboxes and charging stations, with Modbus®-capable meters and Docker®-capable controllers. WAGO Application Load Management can be used, for example, to manage charging parks of any size or integrate a wide variety of loads and control them in a way that avoids peak loads. The new native MQTT interface supports connection to the WAGO Solutions Platform or other cloud-based platforms. The standard interface of the WAGO Application Customer Substation allows configurable connection of EEG systems for mixed parks based on the technical connection rules (TCRs) of network operators.

  • Optimal utilization of charging infrastructure
  • Dynamic control offers a higher charging point power than the available grid connection power.
  • Great openness to interfaces and brands

A Look at the Software

Intuitive meter configuration via drop-down menu

Clear display of the charging park and status messages of the charging points – also available as a list view

Settings for all relevant electrical parameters of the charging station in an input screen

Convenient selection from a drop-down menu of pre-integrated charging stations and wallboxes and connection parameters; the OCPP forwarding settings can be selected individually for each charging point.

Advantages of the WAGO Application Load Management

AC/DC Charging Parks

  • For small, medium or large charging parks
  • 1 to 225 charging points per controller
  • Combination of fast loaders, charging stations and wallboxes
  • Power of integrated charging stations: 11 kW to 350 kW
  • Mixed parks: combining AC chargers and DC chargers

Individual Control

  • Control per charging point, charging group or overall park
  • Merge charging points into charging groups
  • Individual adaptation to the electrical infrastructure, taking into account the connection power
  • Prioritization of different charging points and groups

Integration of Inverters for PV and Storage Systems

  • Consideration of renewable energies and storage systems
  • Support for the Sunspec protocol
  • Increase performance availability through PV and storage integration
  • Excess PV charging and charging from 100% self-generated energy possible

WAGO Charging Park Management

WAGO Charging Park Management consolidates key information and the current status of multiple charging parks. It ensures an intuitive and efficient management experience for all users.

WAGO Load Management Controller

WAGO Load Management Controller: Unpack and load. The WAGO Load Management Controller with the pre-installed Load Management Application on the WAGO Compact Controller 100. An additional connection to a network operator or building management is possible.

Advantages:

  • Software is already installed
  • Easy parameterization via Web browser
  • Select compatible charging stations and hyperchargers from the drop-down menu
  • The charging park can be flexibly regulated using digital inputs

MM-22719_website_compact-controller-100_0751_9301_p1_2000x1125.jpg

Manufacturer-Independence

Compatible Charging Stations and Wallboxes

WAGO Application Load Management is compatible with the following charging stations and wallboxes, among others: ABB, ABL, Alfen, Compleo, Delta, Keba, Mennekes, Schneider and Technagon. A complete list is available here:

MM-484030_website-update-Integration-kompatible-Ladepunkte_charger_2000x1125.jpg

Compatible Meters

The software solution is compatible with the following electricity meters: ABB, Eastron, EMU, Hager, Janitza, Kostal, PQ Plus, Siemens, Socomec, TIP and WAGO. You can find more information in this complete list:

MM-484030_website-update-Integration-kompatible-Ladepunkte_energymeter_2000x1125.jpg

Customer Applications

The Signs Point to Current

Experience from the “Green Car Policy” optimizes WAGO Application Load Management.

HAJ: Hit the Ground Running in a Fully Charged E-Vehicle

Since the beginning of the year, enercity has been building publicly accessible charging infrastructure at Hanover Airport, relying on WAGO’s load management. At its core is the WAGO Compact Controller 100.

MM-428829_new_website-page_enercity_walm_gettyimages-1384632126_2000x1125.jpg

Our Products in Use

Energy Measurement Technology

Energy monitoring forms the basis for increasing the efficiency of your energy distribution and processes. Our harmonized energy measurement products save you much effort and expense for energy data collection. Energy meters are suitable for billing-relevant measuring points.

Power Supplies

WAGO’s efficient power supplies always deliver a constant supply voltage – whether for simple applications or automation with greater power requirements. WAGO offers uninterruptible power supplies (UPS), buffer modules, redundancy modules and a wide range of electronic circuit breakers (ECBs) as a complete system for seamless upgrades.

MM-388432_GWA_IF-Categories_Power-Supplies-Systems_01_02_2000x2000.jpg

Switches

WAGO’s range of switches ensures the scalability of your ETHERNET network infrastructure, while providing outstanding electrical and mechanical performance. These rugged switches are designed for industrial use and are fully compliant with IEEE 802.3, IEEE 802.3u and IEEE 802.3ab.

mm-172328_switche_2000x1125.jpg

FAQ – Questions and Answers about E-Mobility
and Load Management for Charging Infrastructure

A load management system for charging infrastructure allows the expansion and integration of e-mobility into power grids. Load management for EV charging controls the power of multiple charging points in order to optimize utilization of the existing existing grid connection – without the need for a power rating increase or even a new transformer at the grid connection point. Therefore, where there are multiple charging points, a load management system is usually necessary for integration of the charging infrastructure, because buildings, parking lots and underground garages are generally not designed with large power reserves.

Static load management is the simplest kind of load management system, where a preset static energy value is available to all loads. Static load management does not take any other consumers or generators into account.

An example of static load management for charging infrastructure:

Three charging stations are available with a total capacity of 22 kilowatt hours. If only one electric vehicle is charging at the three charging stations, it can be charged at the full 22 kilowatt hours. If two vehicles are connected, these 22 kilowatt hours are distributed equally among the two charging points.

Dynamic load management differs from static load management in one fundamental respect: The available energy is no longer static, but variable. In dynamic load management for charging infrastructure, the capacity is measured and dynamically distributed among the charging stations. For example, if the sun shining on solar power installations that feed into the grid, the total available charging power at the charging stations is increased to optimize utilization of the available electricity.

From the energy industry’s point of view, load management is necessary in order to keep grids stable and ensure security of supply. In the area of e-mobility, this means supplying the growing charging infrastructure with the additional electricity it needs without overloading the grid interconnection points. This requires generation and consumption – as well as storage, if applicable – to be harmonized. But renewable energy from decentralized generators fluctuates. Therefore, it is important to use surplus energy in the grid through flexible loads. This is exactly where WAGO comes in. Load management regulates the flow of energy and controls all loads, energy storage systems and generators in the energy network.

In addition to the cost of energy consumed, industrial and commercial companies and large properties whose consumption exceeds 100 megawatt hours (MWh) must pay a so-called demand charge: the price that has to be paid if the set power limit is exceeded. For the demand charge, the maximum average power consumption is calculated at a quarter-hour intervals. Normally, the quarter hour with the highest mean value is applied to the whole year. For example, with a demand charge of 110 euros per kilowatt (kW), a load peak of 1,000 kW can lead to additional annual costs of 110,000 euros. With the integration of a charging infrastructure for e-mobility, an additional consumption factor is added. Therefore, intelligent load management for energy flows is extremely important, especially for preventing peak loads (so-called “peak shaving”) in order to avoid additional costs.

Energy management is a higher-level system in which all load currents of consumers and generators are continuously measured, monitored and optimized. Energy management systems are used in intelligent networks such as smart grids, microgrids and nanogrids to improve energy efficiency. This includes real estate, industrial companies and even utilities. A fundamental goal is to minimize the consumption of auxiliary materials, additives and raw materials. Load management for charging infrastructure ensures a sensible distribution of existing loads within the energy management. So load management is only part of an overall energy management package – albeit an important one.

Aiheeseen liittyvää: